Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

vaciar (v)

Gießen (n)

cast (v)


The smooth-running castors incorporate reliable braking mechanisms.

The castors are on and the panel is being fitted now.

Another option is to use a lockable container on castors.

casting (n)


A distinction is made between casting in a permanent mould and expendable mould.

The castings fall out of the mould once the vacuum is released.

Afterwards, the shape and dimensions of the casting no longer resemble the original ingot.

pour (v)


The electrons penetrate deeply into the material, creating a narrow, tubular vapour channel.

Light effect - electric current causes certain gases (neon, argon, mercury vapour) to light up.

Once the melt has been poured into the mould, solidification can be straight-walled, rough-walled and sponge-like (exogenous solidification) or shell-forming (endogenous).

pouring (n)


In the case of vacuum forming, a vacuum is used to deep draw a film over the model for a one-off (expendable) mould and a pouring basin and feeder are formed.

浇铸 (n)

铸造 (v)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web