一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

铸造 (v)

Gießen (n)

cast (v)


The smooth-running castors incorporate reliable braking mechanisms.

The castors are on and the panel is being fitted now.

Another option is to use a lockable container on castors.

casting (n)


A distinction is made between casting in a permanent mould and expendable mould.

The castings fall out of the mould once the vacuum is released.

Afterwards, the shape and dimensions of the casting no longer resemble the original ingot.

pour (v)


The electrons penetrate deeply into the material, creating a narrow, tubular vapour channel.

Light effect - electric current causes certain gases (neon, argon, mercury vapour) to light up.

Once the melt has been poured into the mould, solidification can be straight-walled, rough-walled and sponge-like (exogenous solidification) or shell-forming (endogenous).

pouring (n)


In the case of vacuum forming, a vacuum is used to deep draw a film over the model for a one-off (expendable) mould and a pouring basin and feeder are formed.

vaciado (n)

vaciar (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站