Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

iniciar (v)

einleiten (v)


Andererseits ist die Auflagefläche groß genug um eine plastische Verformung an den Kraft einleitenden Flächen zu verhindern.

initiate (v)


After a certain delay, the material flow is initiated and starts to head back toward the final production stage.

Once there are no cards left to initiate a production flow, the company has achieved a one-piece flow (OPF).

It initiates internal forces in an element that are distributed over the component's cross-section and length.

start (v)


Capacities then started to become available for the production of consumer goods.

The roller tool is now ready to start beading the upper ribs.

The return stroke (non-cutting stroke) returns the tool to the starting position.

发起 (v)

开始 (v)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web