一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

发起 (v)

einleiten (v)


Andererseits ist die Auflagefläche groß genug um eine plastische Verformung an den Kraft einleitenden Flächen zu verhindern.

initiate (v)


After a certain delay, the material flow is initiated and starts to head back toward the final production stage.

Once there are no cards left to initiate a production flow, the company has achieved a one-piece flow (OPF).

It initiates internal forces in an element that are distributed over the component's cross-section and length.

start (v)


Capacities then started to become available for the production of consumer goods.

The roller tool is now ready to start beading the upper ribs.

The return stroke (non-cutting stroke) returns the tool to the starting position.

iniciar (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站