Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

hendidura (n)

Einkerbung (f)

groove (n)


Some cross-sections incorporate closed grooves that can be easily opened.

It can also be used to safely cover over cables that have been routed through a groove.

Profile Tubes are available with up to four grooves according to requirements.

indent (n)


A connection can also be made with panels using the drill indentations.

A stiletto heel tip will leave indentations in a wooden floor.

nick (n)


Verbundmaterial ist schubsteif und hat hohe Biege- und Knickfestigkeit.

Die Kraft, ab der der Knickvorgang beginnt, wird als Knickkraftbezeichnet.

Die Verrundung der innenliegenden Kante verhindert  ein Abknicken der Leitungen.

notch (n)


In the notched bar impact test, the test specimen is called a notched specimen.

The larger the notch radius, the more uniform the flux of force.

A pivoted pendulum hammer is used for the notched bar impact test.

刻痕 (n)

缩进 (n)

缺口 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web