一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

缩进 (n)

Einkerbung (f)

groove (n)


Some cross-sections incorporate closed grooves that can be easily opened.

It can also be used to safely cover over cables that have been routed through a groove.

Profile Tubes are available with up to four grooves according to requirements.

indent (n)


A connection can also be made with panels using the drill indentations.

A stiletto heel tip will leave indentations in a wooden floor.

nick (n)


Verbundmaterial ist schubsteif und hat hohe Biege- und Knickfestigkeit.

Die Kraft, ab der der Knickvorgang beginnt, wird als Knickkraftbezeichnet.

Die Verrundung der innenliegenden Kante verhindert  ein Abknicken der Leitungen.

notch (n)


In the notched bar impact test, the test specimen is called a notched specimen.

The larger the notch radius, the more uniform the flux of force.

A pivoted pendulum hammer is used for the notched bar impact test.

hendidura (n)

mella (n)

muesca (n)

ranura (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站