Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

Umriss (m)


Mit dem Laserstrahl können komplexe Umrisse auch an schlecht zugänglichen Stellen hergestellt werden.

contour (n)


The form of Support Arm X 6-8 corresponds to the clean contour of profile form X.

for the ultimate in functionality, precise contours and no protruding edges.

The special Angle Brackets X Zn and Hinges, heavy-duty X are adapted to profile contour X.

outline (n)


The section on steel tube systems outlines the key features of these products.

The content outlined above is to be presented as usual on the morning of the training day.

The factors outlined here are easy to apply when discussing standalone work benches.

profile (n)


A special Lid Profile is used to seal the conduit.

So it should not be used for profile connections in combination with fastening elements.

Die Innenecke der Winkelprofile ist mit einem Freistich versehen.

轮廓 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web