Seleccione uno
o más idiomas
The smooth-running castors incorporate reliable braking mechanisms.
Some cross-sections incorporate closed grooves that can be easily opened.
For example, rooms can be separated acoustically using special insulation designed to muffle footfall noise.
They can travel at speeds of up to six kilometres per hour.
That helps to speed up the design process for a work bench system considerably.
Brake rollers can be used to limit the speed of descent.
Contemporary styling for profiles and accessories adds a new dimension to mechanical engineering.
The flexible solution when something needs to be attached temporarily.
In the goods issue area, goods are picked and, if necessary, stored on a temporary basis.
During deceleration, the velocity is reduced to V5, V6 and V7.
The following formula shows how wave length , frequency and sound velocity are related: .
Velocity v describes the change in the path s over time t.