Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

tamaño (n)

Maß (n)


Kleine Abmaße zur direkten Montage neben einer senkrechten Strebe.

Die Anordnung der Komponenten folgte einem festgelegtem Rastermaß.

Die Dicke t ist relativ zu den übrigen Abmaßen des Bauteil gering.

dimension (n)


Im dreidimensionalen Raum gelten sechs Gleichgewichtsbedingungen.

There are six conditions of equilibrium in a three-dimensional space.

Small dimensions enable installation directly adjacent to a vertical strut.

gage (n)


When doing so, ensure that all the teeth of the Timing Belt are engaged.

The threaded bore engages with the spindle of a height-adjustable Knuckle Foot.

They have an anti-torsion element which engages with the profile grooves.

gauge (n)


Pressure gauges use both direct and indirect measuring methods.

Examples of such measuring instruments include piston and fluid gauges.

In practice, the strain gauge is used in a measuring bridge and measures the change in voltage.

measure (n)


Positional coordinates are measured constantly to control the vehicle movements.

The Hall voltage can be measured at this potential gradient.

The elongation, that is to say the change in the length of the test member, is measured

size (n)


A person's physical strength will also vary according to their age, body size, weight and gender.

Depending on the profile size and load, several pairs may be necessary.

The height-adjustable work bench - ideal for users of all sizes.

大小 (n)

尺寸 (n)

测量 (n)

量规 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web