Seleccione uno
o más idiomas
This value is referred to as the physical endurance limit for static muscle work.
For fastening Limit Switches to profiles or other components.
The Limit-Switch Holder is also suitable for other linear units.
Dimensional tolerance is defined by the limit sizes - the maximum and minimum dimensions.
The difference between the two limit sizes is the dimensional tolerance, which is also determined by size and position.
A designer will specify the permissible limit sizes for a component - its minimum and maximum dimensions - using the nominal dimension and a dimensional tolerance.