Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

revisión (n)

Prüfung (f)


Dieser Labortisch wurde für die Prüfung von Frontscheiben entwickelt.

Die automatische Überprüfung Ihrer USt.-IdNr. war leider nicht möglich.

Sichtprüfung, ob das Zahnrad mittig in der Profilnute des Trägerprofils läuft.

audit (n)


Schall sind Geräusche, Töne und Klänge, die auditiv mit dem Ohr-Gehirn-System wahrgenommen werden.

Sounds are noises that can be picked up by the auditory system.

check (n)


Also check the maximum load-carrying capacity of the Threaded Inserts.

The same logic is then applied as with check count 1.

The stocktaking manager then also checks whether all stocktaking locations have been covered.

examination (n)


Because value analysis - as a retrospective examination - uses the same tools as design engineering, the two processes complement each other.

gauging (n)


When gauging the maximum permissible loads, all weight forces must be compared against the nominal load-carrying capacity of the fasteners.

When gauging the maximum permissible loads, it is important to compare all weight forces and the nominal load-carrying capacity of the fasteners with regard to friction resistance.

inspection (n)


This lab work bench was developed for the inspection of windscreens.

Carry out a visual inspection to ensure that the end surfaces of all of the Rack Segments meet.

The planned period of use and frequency of inspections are also to be given due consideration.

investigation (n)


The stocktaking manager is to document the result of these investigations on the count list.

screening (n)


Similar guards, enclosures and screening might also be necessary for inspection tasks.

Depending on their specific circumstances, different people will need different types and amounts of screening.

These pinpoint noise zones that require special protective measures (hearing protection, screening).

scrutiny (n)

test (n)


You can now also find our latest catalogues in the App Store.

Tensile testing provides one example of elastic behaviour.

Exceeding the static strength causes necking of the tensile test specimen.

verification (n)

审计 (n)

检查 (n)

测定 (n)

确认 (n)

筛选 (n)

试验 (n)

详细审查 (n)

调查 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web