Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

compresión de resorte (n)

Einfederung (z.B. Feder) (f)

compliance (n)


The door can be opened and closed in full compliance with machine design directives.

Systematic quality management ensures complete compliance with agreed standard values.

The strength of rolling friction varies according to the surface attributes, compliance and hardness of the rolling element and surface.

contraction (n)


This elongations a right angles to the direction of traction is called lateral contraction.

This narrowing is referred to as lateral contraction, which is dependent on the Poisson ratiov.

The Poisson number is a dimensionless parameter for a body's lateral contraction under a tensile stress.

deflection (n)


However, deflection in the Shaft is even more important.

Profile deflection caused by the inherent load and the load from the assemblies.

Profile deflection in very wide work benches due to the weight of the bench itself.

resilience (n)

spring compression (n)

偏差 (n)

合规 (n)

弹性 (n)

弹簧压缩 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web