Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

nivel máximo (n)

Obergrenze (f)

ceiling (n)


The ceiling construction reaches from one side of the room to above the operating table.

The ceiling mount can be seen in the background, running from left to right into the room.

The ceiling mount made of MB profiles was installed in next to no time and the mobile camera was almost ready for use.

maximum level (n)

upper limit (n)


In this case, the actual value oscillates around the setpoint value, because the manipulated variable jumps to '1' if it falls below a certain value and to '0' if it exceeds the upper limit value.

上限 (n)

最大水位 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web