Seleccione uno
o más idiomas
Auch an metallurgischen Kerben wie etwa an Schweißverbindungen entstehen Kerbwirkungskräfte.
Bereits die Urmenschen ritzten Kerben in Baumstümpfe ein, welche Sie dann als Stufen nutzten.
Eine Kerbwirkung tritt z. B. an Kerben (konstruktionsbedingten Querschnittsänderungen) eines Bauteiles auf und schwächt dieses.
Some cross-sections incorporate closed grooves that can be easily opened.
It can also be used to safely cover over cables that have been routed through a groove.
Profile Tubes are available with up to four grooves according to requirements.
In the notched bar impact test, the test specimen is called a notched specimen.
The larger the notch radius, the more uniform the flux of force.
A pivoted pendulum hammer is used for the notched bar impact test.
Slot the carriage onto the ready-prepared Profile.
They can be adjusted to the thickness of the panel elements by means of mounting slots.
T-Slot Sliders and Slide Guides for simple guides along the profile grooves.