Seleccione uno
o más idiomas
Bei Fahrzeugbewegungen werden die Lagekoordinaten ständig gemessen.
Endgültig wird das Gebäude für das statistische Kataster eingemessen.
Der angemessene Sehabstand ist abhängig von der Größe des Bildschirms.
Pressure gauges use both direct and indirect measuring methods.
Examples of such measuring instruments include piston and fluid gauges.
In practice, the strain gauge is used in a measuring bridge and measures the change in voltage.
Positional coordinates are measured constantly to control the vehicle movements.
The Hall voltage can be measured at this potential gradient.
The elongation, that is to say the change in the length of the test member, is measured