Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

medios (pl)

Mittel (npl)


Die Schalter werden mittels Klemmung in der Aufnahmenut gehalten.

Am Arbeitsplatz wird mittelgrobe oder Präzisionsarbeit gefordert.

Montiert werden diese mittels Innsensechskant-Schlüssel der SW 5.

means (pl)


The latter option means that Cable Duct E can then be fitted between the columns.

A hand-rail is the primary means of preventing a fall and a useful aid when climbing stairways.

The wires are held securely in the socket by means of a spring-force connection.

resources (pl)


Important resources are used every time a workpiece is moved from one place to another.

Indeed, the only processes that are eliminated are those that use up resources without contributing to the value of the product.

As a result, these systems embody the principles of lean production, which strive for flexibility, economical use of resources and maximum quality.

资源 (pl)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web