Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

inclinación (n)

Steigung (f)


In industriellen Anlagen sollte dieser Steigungswinkel bevorzugt werden.

Die Steigung des Graphen entspricht der momentanen Beschleunigung des Körpers.

Die Neigung des Werkzeuges zur Werkstückachse muss der Gewindesteigung entsprechen.

ascent (n)

gradient (n)


The gradient on the shelves ensures that loads slide down to the removal point.

The Hall voltage can be measured at this potential gradient.

The fastener remains flexible, which means that if gradient a should change at a later point in time, it can be adjusted accordingly.

inclination (n)


The inclination is set in the same way as the Adjustable Stand Foot, using a set screw.

It is particularly suitable for adjusting the height or inclination of equipment.

Outer profile for constructing telescope profiles of variable length for adjusting the height or inclination of fixtures and equipment.

incline (n)


Inclined groove flanks for industry-standard fastenings that offer long-term stability.

The ESD-safe Tray is fitted at an incline using Angle Locking Bracket (A).

This mobile rack has two inclined removal slopes that function as feed-in levels and are positioned at optimum reaching height.

lead (n)


Conduits for Cables and Leads, Profiles with Integrated Conduits ...

Team leaders are nominated, as are sponsors, guides and team members.

In extreme cases, it can lead to head-related illnesses (cramps, collapse, heatstroke).

pitch (n)


This pitch should be favoured in industrial facilities.

The pitch of the line corresponds to the acceleration of the body at any one time.

TPS incorporates various Assembly Sets for a range of stairway pitches and installation scenarios.

slope (n)


An I element's step response is a straight line that rises over time with the slope .

This mobile rack has two inclined removal slopes that function as feed-in levels and are positioned at optimum reaching height.

The amplitude of the output signal depends on the slope of the step function in the range to .

上升 (n)

倾斜 (n)

斜坡 (n)

梯度 (n)

节距 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web