Seleccione uno
o más idiomas
Aus der 2. Bredtschen Formel ergibt sich die Verdrillung des Bauteils, welche von dem Schubmodul G des Werkstoffes abhängig ist.
The deformation depends on the twisted component's cross-sectional geometry.
The worker can reach everything within this zone without having to twist his or her torso.
To remove and then refit the spring clip, twist it in or out of position and lock it in place.
Diagonal struts stabilise the frame construction against twisting and support the Roller Conveyors.
This relationship between work of deformation and displacement/twisting applies only to Hooke's materials.
Torsion is a load state that causes twisting ? due to the action of a torsional moment MT.