Seleccione uno
o más idiomas
An Fatigue test under operational stresses is required when developing plant, machinery, individual components and the associated connections.
It is intended to confirm that the components or assemblies will keep working correctly and safely in continuous operation throughout their calculated service life. Static, dynamic and random loads are included in the test. The dynamic loads may be periodic or impact loads. Environmental influences (temperature, Humidity, corrosive media, radiation, etc.) are also taken into account.
Proof needs to be provided that plant and machinery can withstand the loads in any situation, including exceptional events.
Strength under operational stresses (sometimes referred to as engineering strength) is defined based on behaviour vis-à-vis: