Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

etapa (n)

Stufe (f)


Circle of curvature on a trajectory
Circle of curvature on a trajectory

Die stufenlose Neigungswinkeleinstellung erleichtert die Entnahme.

Das Stufendistanzprofil stellt eine formschlüssige Verbindung her.

Zur Erhöhung der Trittsicherheit sind die Stufenprofile geriffelt.

stage (n)


Trajectory of a projectile without air resistance
Trajectory of a projectile without air resistance

Seven different types of wastage have been identified in production.

Assembly is usually the final stage in a manufacturing process.

It is advisable to use an additional safety factor of 2 at the design stage.

step (n)


Translation of a spherical body
Translation of a spherical body

The Step Spacer Profile establishes a rigid connection.

The next step is to screw the Reverse Unit to the Housing Profile.

Work benches should feature a stepless height-adjustment system that can be operated easily by users with limited physical strength.

步 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web