Seleccione uno
o más idiomas
When doing so, ensure that all the teeth of the Timing Belt are engaged.
The threaded bore engages with the spindle of a height-adjustable Knuckle Foot.
They have an anti-torsion element which engages with the profile grooves.
Companies often fail to understand that the broad diversity of methods and processes in lean production form a single intermeshed entity - isolated applications do not yield optimum results.
The processes employed depend on the state of the materials.
Dies hat eine Materialveränderung (zum Beispiel Härte) zur Folge.
This brings about a change in the material (e.g. hardness).
Black Steel Meshes are also powder-coated at the factory.
Black Dual-Rod Meshes are also powder-coated at the factory.
The bright zinc-plated surface of the Steel Meshes protects them against corrosion.