Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

fricción cinética (n)

Gleitreibung (f)

dynamic friction (n)

kinetic friction (n)


A body can be subjected to kinetic friction on both a level surface and an inclined surface.

The kinetic friction force FK travels in the opposite direction to the sliding body and parallel to the sliding surface.

A body on an inclined plane will move down the slope if the downhill force FD is greater than the kinetic friction force FK.

sliding friction (n)


They can be fitted into the profile grooves, are hard-wearing and have a low coefficient of sliding friction.

The Slide Strips serve as slide elements when transporting goods or workpiece carriers, for example. They can be fitted into the profile grooves, are hard-wearing and have a low coefficient of sliding friction.

动摩擦 (n)

滑动摩擦 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web