Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

desabrochar (v)

lösen (Verbindung trennen) (v)

detach (v)


Easy, safe and detachable solutions for fastening frames in enclosures and guards.

Ensure that no cables, connections or components are detached or removed.

They should be sufficiently stable but easily detachable for when the bench needs to be reconfigured quickly.

disconnect (v)


Always disconnect the Light Fitting from its power source before conducting any maintenance or repair work.

As a result, profiles can be connected in seconds and disconnected just as quickly, with the components then being available for other uses.

separate (v)


For example, rooms can be separated acoustically using special insulation designed to muffle footfall noise.

Es kann aber auch eine separate Bohrung mit ? 7 mm angelegt werden.

However, a separate hole with a diameter of 7 mm can also be created.

unbolt (v)

undo (v)


The tube connection cannot be repositioned without first undoing the entire joint.

Grundobjekte In diesem Bereich des Menübands können die Tischgestelle und SystemMobile verschoben, gedreht und gelöscht werden.

There is also the option to undo the last action or launch an animation of various components.

unfasten (v)


Several struts have to be fastened in place or unfastened at the same time - meaning the entire structure has to be rebuilt or disassembled.

unscrew (v)


After the rivet has been tightened, the tension bolt is unscrewed out of the nut when the trigger is pulled again.

You can shorten the Timing Belt if necessary by unscrewing the Cover Plate, shortening the Timing Belt and refitting it.

Universal lightweight hinge for doors and lids. Can be mounted on the inside or outside of the door (when mounted on the inside it cannot be unscrewed).

分离 (v)

单独 (v)

取下螺栓 (v)

拆卸螺栓 (v)

撤消 (v)

断开 (v)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web