Seleccione uno
o más idiomas
Application 3: supplied square nut is inserted into both collar halves.
The upper surface of the slide has been milled flat and features four openings for positioning collars.
When the clamp collars are aligned in parallel, this indicates that the screw connections are correctly pre-tensioned.
Die Innenecke der Winkelprofile ist mit einem Freistich versehen.
Kanal-Innenecken, -Abdeckkappen und -Durchführungen - Kurvenlage.
Exceeding the static strength causes necking of the tensile test specimen.