Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

Compression test


Test setup for the compression test
Test setup for the compression test

The compression test is a Material testing method used to establish the behaviour of metallic materials that are subject to a uniaxial compressive stress distributed uniformly over the cross-section. A cylindrical compression specimen with a defined initial section is compressed, and the compressive Force is measured and depicted in a force-compression curve. Compression tests are used to calculate compressive stress, which can be determined based on the force in relation to the initial cross-section.

They are used far less often than tensile tests, primarily to determine the compressive Strength of brittle materials or Bearing metals.

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web