Seleccione uno
o más idiomas
Semi-conductors are NTC thermistors, i.e. their resistance decreases as the temperature increases.
Acceleration metrology is used to determine the increase and decrease in the velocity of bodies.
Reversing the polarity of the voltage applied increases the potential barrier and the diffusion decreases exponentially.
The all-round frame stops the materials or tools from dropping off the panel.
The molten droplets are compacted on the receiving surface to form a solid structure.
A drop in the velocity of a body over time is referred to as deceleration.
Die Wettbewerbsfähigkeit hat sich auf jeden Fall hier gesteigert.
Indeed, some regions are already experiencing a shortfall in workers.
For example, rooms can be separated acoustically using special insulation designed to muffle footfall noise.
Mesh and elevated side frames ensure that stored goods do not fall off the racks.
To ensure that granular goods do not fall off the sides of the conveyor, angled rollers can be installed at regularly spaced intervals to give the belt a trough-like shape.