Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

jaula de elevación (n)

Fahrkorb (Aufzug) (m)

cab (n)


If the carriage is to move, a cable chain is required.

Conduit Inside Corners, Conduit Caps and Cable Entry Protectors - Safe cornering.

It can also be used to safely cover over cables that have been routed through a groove.

cabin (n)


Everything from the most awkward corner to large cabins can be lit up.

The under-bench cabinet is ideal for storing tools or housing a PC or other components.

The model is subsequently hardened in a hardening cabinet until it reaches its final strength.

car (n)


If the carriage is to move, a cable chain is required.

Slide the prepared carriage onto the support rail.

The closed side panel gives the Angle Bracket its high load-carrying capacity.

elevator cage (n)

elevator car (n)

lift cage (n)

lift car (n)


The lift carriage in the inner frame also runs on rollers.

Guide rollers are mounted on the two vertical sides of the lift carriage.

电梯轿厢 (n)

舱 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web