Seleccione uno
o más idiomas
The Bending test is a destructive Material test method.
Various test structures are available. They differ according to the number of load applications and the way test pieces are supported.
The bending Force and deflection are recorded. These values can be depicted graphically in a sample-specific stress-strain curve from which material characteristics such as flexural Strength and fracture Toughness can be read off. The flexural strength is the maximum outer fibre stress that a material supports when subjected to an elastic bending stress.