Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

arandela espaciadora (n)

Distanzscheibe (f)


Je nach Anwendungsfall müssen die Distanzscheiben im Gehäuse gedreht werden.

Die unterschiedlichen Dicken der Flächenelemente (von 4 bis 8 mm) können durch die Distanzscheibe ausgeglichen werden.

shim (n)


Spring-tempered shims are not recommended for making adjustments as they can break and damage the drive.

This principle has been taken from glazing, where shims are used to fill gaps between the frame and the glass panel.

If it is not, correct the position by placing a shim between the non-adjustable Bearing Unit and the casing fastening bracket. The shim must be removed once the appropriate adjustments have been made.

spacer (n)


The Step Spacer Profile establishes a rigid connection.

Depending on the particular application, it may be necessary to rotate the spacer washers in the housing.

In conjunction with spacer rings, Hinges, heavy-duty are freely movable.

spacer washer (n)


Depending on the particular application, it may be necessary to rotate the spacer washers in the housing.

The different thicknesses of panel elements (4 to 8 mm) can be compensated using the spacer washer.

垫片 (n)

薄垫片 (n)

间隔垫圈 (n)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web