Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

aplicar (v)

einfallen (Bremse) (v)

be applied (v)


This method can be applied universally and without any great technical effort.

Careful pressure must be applied to lock them into the profile groove.

Loads may only be applied to the Chemical Fixing Bolt after the reaction time has expired.

engage (v)


When doing so, ensure that all the teeth of the Timing Belt are engaged.

The threaded bore engages with the spindle of a height-adjustable Knuckle Foot.

They have an anti-torsion element which engages with the profile grooves.

啮合 (v)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web