Seleccione uno

o más idiomas


0,1,3
  • Alemán
  • Inglés
  • Chino
  • Español

alojar (v)

einbauen (v)


Und das kann das System eigentlich auch ganz gut, auch wenn wir noch zukünftige Innovationen einbauen wollen, da denk ich mal, sind wir auch ganz gut aufgestellt.

Lagersätze für Rollen sind neben der angetriebenen auch in nicht angetriebener Ausführung erhältlich, um z. B. Staurollen in eine angetriebene Rollenbahn einbauen zu können.

build in (v)


Line XMS is used to build inherently stable constructions within which separate functional cells can be created (service, process and supply sections).

fit (v)


Sturdy Light Fitting for illumination of workplaces and machines.

The Arm Rest is fitted to the front edge of the table top.

Always disconnect the Light Fitting from its power source before conducting any maintenance or repair work.

house (v)


This section houses the machine functions and interlinked production steps.

This activity can also be carried out in in-house training facilities.

The lower section houses assemblies and cable and hose connections.

incorporate (v)


The smooth-running castors incorporate reliable braking mechanisms.

Some cross-sections incorporate closed grooves that can be easily opened.

Shelves can be incorporated into the SystemMobile with millimetre accuracy.

install (v)


Processing the panel element for installing the Locking Systems.

Simple aluminium conduits for installation of cables and hoses.

Install the End Cap and Lubricating Systems on the bearing units.

integrate (v)


Conduits for Cables and Leads, Profiles with Integrated Conduits ...

The corresponding ESD Earthing Terminal with integrated 1 mega ohm resistors.

Bosch has integrated the relevant components into its Eco-Shape range.

mount (v)


Place the pulley over the guide pin onto the mounting plate

Its ball-bearing mounted pulleys ensure quiet and smooth running over long-term use.

The latter allows users to mount the drive on the slide.

内置 (v)

安装 (v)

房屋 (v)

组合 (v)

配合 (v)

集成 (v)

Búsqueda adicional


item


Descubra soluciones innovadoras para
la construcción de máquinas y la automatización.

A la página web