一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

过程 (v)

behandeln (v)


Eine ansprechend gestaltete Arbeitsumgebung erhöht zudem die Bereitschaft der Mitarbeiter, ihre Arbeitsplätze pfleglich zu behandeln.

Eine ansprechend gestaltete Arbeitsumgebung erhöht zudem die Bereitschaft der Mitarbeiter, ihre Arbeitsplätze pfleglich zu behandeln.

Eine ansprechend gestaltete Arbeitsumgebung erhöht außerdem die Bereitschaft der Mitarbeiter, ihre Arbeitsplätze pfleglich zu behandeln.

handle (v)


Handles Al can be secured from the rear (concealed).

We offer presentation platforms for all easy-handle exhibits / display cubes.

Handles T are ESD-safe and available in a range of lengths.

manipulate (v)


Everything can be manipulated or by-passed in some way - however it must not be easy to do so.

Use the navigation icons at the bottom edge of the screen to manipulate the view freely.

The controlled system's parameters can be determined from its reaction to the change in the manipulated variable.

process (v)


Processing the panel element for installing the Locking Systems.

Parts can changed repeatedly throughout the work process.

This process involves tensile and bending deformation.

treat (v)


The model is usually made of metal, plastic or treated wood.

And that is why the logistics of each work bench must be treated as a part of the production process.

The work bench must be treated as a dynamic position that is manned by a moving human employee.

work (v)


Sturdy Light Fitting for illumination of workplaces and machines.

Always set down the height-adjustable work bench on a level surface.

The transfer systems are permanently connected to the work benches.

manejar (v)

manipular (v)

trabajar (v)

tratar (v)

进一步查找


item


访问 item 官网
我们的新网站

去網站