Wählen Sie eine
oder mehrere Sprachen aus
Halbwarmschmieden verringert das Verzundern der Oberfläche, allerdings unter Einsatz höherer Kräfte.
A scale fitted on the Reverse Unit can be used to verify that the two screws are tightened evenly.
Machine moulding is primarily suited to medium-size and large-scale production.
The scale embossed on the side of the Reverse Unit indicates the tensioning axle travel.
Warm forging reduces surface scaling but higher forces must be applied.