Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

tragend (adj)


Bei höherer Tischlast wird das tragende Horizontal-Rohr verdoppelt.

Die vielen tragenden Kugeln der Kugelrollenführung ist deutlich im Vorteil.

Die vielen tragenden Kugeln der Kugelrollenführung sind deutlich im Vorteil.

bearing (adj)


Its ball-bearing mounted pulleys ensure quiet and smooth running over long-term use.

Install the End Cap and Lubricating Systems on the bearing units.

The fixed bearing must be positioned on the drive side of the Conveyor Roller.

carrying (adj)


The closed side panel gives the Angle Bracket its high load-carrying capacity.

When working with higher table loads, the load-carrying horizontal tube is doubled.

Also check the maximum load-carrying capacity of the Threaded Inserts.

load-bearing (adj)


Pallet jacks have a load-bearing capacity of two to three metric tons.

All connections become stable and load-bearing as soon as they have been tightened.

This translates into a high load-bearing capacity that resists displacement.

supporting (adj)


There is no need for supporting structures in micro-stereolithography.

Also ideal for creating supporting beams for panels, etc.

Clean the Shaft-Clamp Profiles and the groove in the supporting profile.

承载 (adj)

支持 (adj)

轴承 (adj)

cargando (adj)

portar (adj)

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!