Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

Lauf (m)


Dadurch ruhigerer Lauf, schont sensible Produkte (wenig Rumpeln).

Auch Kabel, die in der Nut verlaufen, können so geschützt werden.

Ihre wälzgelagerten Riemenscheiben sorgen dauerhaft für Laufruhe.

motion (n)


During this infinitesimally short moment in time, it is motionless.

The tilting motion determines the path of motion of the goods as they are ejected.

In this state, the body is either motionless or moves at a uniform speed in a straight line.

movement (n)


Planning must ensure that unnecessary, monotonous movements are avoided.

Movement along the X axis is controlled by two synchronised KLE 8.

Positional coordinates are measured constantly to control the vehicle movements.

operation (n)


It is not intended for continuous lifting operations in automated industrial processes.

Long 'cycle times', removal operations can be interrupted, restricted space

Auxiliary tools are also required occasionally in packaging operations.

running (n)


The smooth-running castors incorporate reliable braking mechanisms.

Its ball-bearing mounted pulleys ensure quiet and smooth running over long-term use.

The electronic system monitors how long the drives have been running.

service (n)


Space saving, with a long service life and low maintenance.

easy-running roller conveyors with steel axles for a long service life.

Ersetzen Sie die Steuerung, oder rufen Sie Ihren Servicepartner an.

travel (n)


They can travel at speeds of up to six kilometres per hour.

Due to high wheel forces, travelling wheels installed in cranes have broad running surfaces.

The travelling wheels of very large cranes are often driven individually.

操作 (n)

服务 (n)

移动 (n)

行程 (n)

运动 (n)

运转 (n)

funcionamiento (n)

movimiento (n)

operación (n)

servicio (n)

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!