Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

Resistance


Electrical - or ohmic - resistance occurs when moving charge carriers collide with Conductor atoms. This impedes uniform charge carrier motion - the current flow. The greater the conductor material's cross-section, the lower the conductor's resistance. This is because the electrons have more space in the conductor with the same current intensity (= same number of charge carriers), so there are fewer collisions with the metallic lattice. Similarly, the resistance increases with the length of the conductor, because a Collision is more likely over a longer distance.

In the case of metallic conductors, resistance increases as the temperature rises (PTC resistor). Semi-conductors are NTC thermistors, i.e. their resistance decreases as the temperature increases.

In mathematical terms, the electrical resistance R expresses the relationship between voltage V and current I. In a circuit with ohmic resistance only, Ohm's law applies: $R = V/I$. In an electrical circuit with inductances or capacitances, the Impedance is derived from the effective resistance and the reactance.

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!