Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

Material testing


Material tests are primarily used to determine a material's properties in research and development applications, to perform checks and Quality assurance measures during production and to analyse any damage.

Essentially, test methods can be split into the following groups:

  • Mechanical, physical and chemical analyses
  • Testing of characteristic values and material/processing properties (material analysis)
  • Structural analysis
  • Troubleshooting.

In most cases, tests are performed on test pieces (samples). A distinction is made between destructive and non-destructive test methods, and also between static methods with constant or slowly increasing loads and dynamic methods with sudden or periodic loads.

In the case of mechanical test methods, a differentiation is made according to the type of load. Examples include compression, tensile, Torsion, Bending, vibration (fatigue), notched-bar and shear tests. Burning tests, gas chromatography, crystallography and end quench tests are all examples of chemical and thermal testing.

Non-destructive test methods include Strain gauge, ultrasonic and radiographic testing, infrared thermography and also visual inspection.

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!