Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

ineinander greifen (v)

engage (v)


When doing so, ensure that all the teeth of the Timing Belt are engaged.

The threaded bore engages with the spindle of a height-adjustable Knuckle Foot.

They have an anti-torsion element which engages with the profile grooves.

intermesh (v)


Companies often fail to understand that the broad diversity of methods and processes in lean production form a single intermeshed entity - isolated applications do not yield optimum results.

mate (v)


The processes employed depend on the state of the materials.

Dies hat eine Materialveränderung (zum Beispiel Härte) zur Folge.

This brings about a change in the material (e.g. hardness).

mesh (v)


Black Steel Meshes are also powder-coated at the factory.

Black Dual-Rod Meshes are also powder-coated at the factory.

The bright zinc-plated surface of the Steel Meshes protects them against corrosion.

使互相啮合 (v)

使配对 (v)

啮合 (v)

acoplar (v)

entremallar (v)

mallar (v)

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!