Wählen Sie eine
oder mehrere Sprachen aus
Die Innenecke der Winkelprofile ist mit einem Freistich versehen.
Kanal-Innenecken, -Abdeckkappen und -Durchführungen - Kurvenlage.
Exceeding the static strength causes necking of the tensile test specimen.
The Captive Nuts can be installed by snapping the latch springs into the corresponding recess.
As a result, they run on the top and underside of the recess in the support profile.
The closed rear wall of the Recessed Grip prevents the operator's fingers from extending all the way through and possibly being injured.