Wählen Sie eine
oder mehrere Sprachen aus
You are using only original equipment from the manufacturer.
The relevant equipment also has to be installed at the work bench.
The U-shaped fork arms are equipped with small load rollers.
Sturdy Light Fitting for illumination of workplaces and machines.
The Arm Rest is fitted to the front edge of the table top.
Always disconnect the Light Fitting from its power source before conducting any maintenance or repair work.
Also check the maximum load-carrying capacity of the Threaded Inserts.
Insert the set nuts into the corresponding cavities in the carriage profile.
It is inserted into the grooves of adjacent Step Profiles.
Sturdy Light Fitting for illumination of workplaces and machines.
Place the pulley over the guide pin onto the mounting plate
The profiles can then be fixed in place using the three grub screws.