Wählen Sie eine

oder mehrere Sprachen aus


0,1,0
  • Deutsch
  • Englisch
  • Chinesisch
  • Spanisch

Bauteil (n)

component (n)


Special components are available for these guard units.

The variable t represents the wall thickness of the thin-walled component.

The components were arranged according to a specific modular dimension.

element (n)


Daher ist er zum Einsatz mit Verbindungselementen nicht geeignet.

So it should not be used for profile connections in combination with fastening elements.

Bearbeitung des Flächenelements zum Einbau der Verschlusssysteme.

member (n)


In fixed supports (valency of 3), the member is always tangentially adjacent.

A truss is a structure comprising several members.

The elongation, that is to say the change in the length of the test member, is measured

part (n)


There must be a simple method of delivering parts to the work bench.

Parts can changed repeatedly throughout the work process.

Über einen Pulverstrahl können feste Partikel beigemischt werden.

structural component (n)


Fastening elements for panelling elements, working surfaces, steps, information provision and container mountings enhance the structural components.

Endless possibilitiesStructural components are enhanced by fastening elements for panelling and working surfaces and for making sureinformation and container mountings are close to hand.

元件 (n)

杆件 (n)

部件 (n)

componente (n)

componente estructural (n)

elemento (n)

miembro (n)

pieza (n)

Weitere Suche


item


Mehr über innovative Lösungen für
Maschinenbau und Automation erfahren Sie hier.

Mehr erfahren!