Wählen Sie eine
oder mehrere Sprachen aus
Panel elements can be slid into the profile groove without needing cutouts in the corners.
Panel elements can be slid into the profile groove without needing cutouts at the corners, where the fastening elements are.
The Captive Nuts can be installed by snapping the latch springs into the corresponding recess.
As a result, they run on the top and underside of the recess in the support profile.
The closed rear wall of the Recessed Grip prevents the operator's fingers from extending all the way through and possibly being injured.