Wählen Sie eine
oder mehrere Sprachen aus
Acceleration causes the sand to adhere closely to the model.
Static friction is a force between two mutually adherent bodies.
The maintenance holes can be cut at any accessible point as long as the cutting ??? dimensions are adhered to.
These small stickers are used primarily for labelling panel elements, roller conveyors, etc.
One way of improving fracture toughness - in aircraft manufacturing, for example - is to stick layered stiffeners onto the sheet metal.
Bauartbedingt neigen Gleitführungen insbesondere bei geringen Geschwindigkeiten und erhöhter Belastung zu leicht ungleichförmigem Lauf (Stick-Slip-Effekt).