一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

输出变量 (n)

Ausgangsgröße (f)

output value (n)


The output value is determined by the speed at which the control error changes.

The stability of a closed-loop control system indicates whether the aim of keeping the output value at the setpoint value is achieved.

A P controller is a transfer element in a closed-loop control system where the output value (manipulated variable y) changes proportionally to the control deviation e.

output variable (n)


Input and output variables can be both analogue and digital.

An actuator is used to influence the output variable depending on the input variable w.

A system's steady-state response is the relationship between the change in the output variable and that in the input variable in the steady state.

variable de salida (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站