一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

斯坦纳(Steiner)定理 (n)

Verschiebesatz (m)


Es entsteht jedoch laut des Verschiebesatzes nicht bei Verschiebung einer Kraft entlang ihrer Wirkungslinie, da Kräfte linienflüchtige Vektoren sind.

parallel-axis theorem (n)


The parallel-axis theorem (Steiner's theorem) is used to transform area moments of inertia onto an axis running parallel to the centroid (gravity) axis.

In the case of components comprising composite cross-sectional areas, the parallel-axis theorem can be used to determine the area moments of the total cross-sections.

However, the parallel-axis theorem states that offset moment is not produced when a force is moved along its line of action, because forces are sliding vectors.

Steiner's theorem (n)

teorema de eje paralelo (n)

teorema de Steiner (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站