一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

过程 (n)

Verfahren (Prozess, z.B. Fertigung) (n)

approach (n)


This innovative approach cuts assembly time and saves a great deal of space in machinery.

That is the most common approach when selecting a linear slide.

This approach ought to take into account the fluctuating demand on the market.

method (n)


This method of delivering information has several advantages.

There must be a simple method of delivering parts to the work bench.

Doch die Methoden, dies zu erreichen, haben sich stark verändert.

practice (n)


In practice, it is not possible to create a completely closed system.

The factory equipment / plant must correspond to generally accepted engineering practices.

In practice, the strain gauge is used in a measuring bridge and measures the change in voltage.

procedure (n)


In the most straightforward of cases, the necessary operating procedures are not visible.

All aluminium profiles can be recycled using procedures which are entirely eco-friendly.

Such documentation normally features standardised layouts and standardised operating procedures.

process (n)


Processing the panel element for installing the Locking Systems.

Parts can changed repeatedly throughout the work process.

This process involves tensile and bending deformation.

technique (n)


Heijunka is a technique for sequencing production and smoothing out fluctuations.

This creates load-bearing structures that combine all the advantages of steel and profile-based building techniques.

Simple cutting and joining techniques are all it takes to build customised structures that meet specific requirements.

método (n)

práctica (n)

procedimiento (n)

proceso (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站