一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

滴 (n)

Abfall (z.B. Spannung, Druck) (m)

dip (n)


Ideally, the seat should dip forward slightly and rotate.

The hot-dip galvanized surface of the Dual-Rod Meshes protects them against corrosion.

Asimaio voloribus de volenim usandest, ommod moloriam faccum cullab idipsae maxim andita as id qui omnimoditia quatem.

drop (n)


The all-round frame stops the materials or tools from dropping off the panel.

The molten droplets are compacted on the receiving surface to form a solid structure.

A drop in the velocity of a body over time is referred to as deceleration.

fall (n)


Die Wettbewerbsfähigkeit hat sich auf jeden Fall hier gesteigert.

Indeed, some regions are already experiencing a shortfall in workers.

For example, rooms can be separated acoustically using special insulation designed to muffle footfall noise.

caída (n)

sumergido (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站