一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

样式 (n)

Gestalt (f)

contour (n)


The form of Support Arm X 6-8 corresponds to the clean contour of profile form X.

for the ultimate in functionality, precise contours and no protruding edges.

The special Angle Brackets X Zn and Hinges, heavy-duty X are adapted to profile contour X.

design (n)


The three design variants have been developed to provide the optimum solution for a range of different applications.

The four design variants have been developed to provide the optimum solution for a range of different applications.

For example, rooms can be separated acoustically using special insulation designed to muffle footfall noise.

form (n)


Diese Art der Informationsübermittlung hat noch weitere Vorteile.

This method of delivering information has several advantages.

The TPS guard-rail system is the perfect complement to the platform system.

shape (n)


The basic shape is based on the geometry of the handling area.

The U-shaped fork arms are equipped with small load rollers.

Bosch hat entsprechende Komponenten im Eco-Shape-Programm integriert.

style (n)


The friendly, informal style of the website is reinforced by the broader use of multimedia content.

The company continued to manufacture specialist machinery, using a 'container-style' modular approach based on standard basic elements in the form of rectangular tubes.

Precision with styleThis spindle drive is the best solution when low travel speeds and exceptional repeat accuracy are called for.

diseño (n)

estilo (n)

forma (n)

进一步查找


item


访问 item 官网
我们的新网站

去網站