一种定义

四种语言


0,1,2
  • 德國
  • 英語
  • 中國
  • 西班牙語

fest (adj)


Die hohe Zugfestigkeit bietet zusätzliche Sicherheit gegen Bruch.

Die Befestigungsscheibe M5 hat eine Sackloch-Bohrung mit Gewinde.

Mit zwei Fixierstücken wird die axiale Lage der Rolle festgelegt.

firm (adj)


Participating staff must confirm that they have been briefed.

An diesem Tisch ist das "Rizo by Light" der Firma Morath verbaut.

Um die Mitarbeiter - das wichtigste Kapital einer Firma - zu schützen.

fixed (adj)


In fixed supports (valency of 3), the member is always tangentially adjacent.

The profiles can then be fixed in place using the three grub screws.

Only the two End Sections are fixed in place using a dowel screw.

solid (adj)


After calendering, the product is solidified on cooling rollers.

Milling is a machining process for solid materials.

In addition, polymer fleece can be solidified to form non-woven fabrics.

stationary (adj)


One of the dies is stationary and the other slides.

Double-brakes on the castors ensure that the trolleys stay safely and securely in place while in stationary use.

The double-brakes on the four smooth-running castors keep the trolley safely in place when in stationary use.

strong (adj)


Hinges Al light are adjustable, strong and versatile.

To provide a stronger hold, it also has to be screwed to the (Profile) Tube.

This rack is extremely strong and yet still easy to move around.

estacionario (adj)

fijo (adj)

firme (adj)

fuerte (adj)

进一步查找


item


访问 item 官网
我们的新网站

去網站