一种定义
四种语言
Aus dem Muster (Punktwolke) des entstehenden Streudiagramms kann erkannt werden, in welcher Abhängigkeit die beiden Merkmale zueinander stehen.
The scatter diagram is one of the "Seven Tools" of quality management.
A scatter diagram is used to display the correlation between two variables as a value pair (x/y).
The pattern (scatter plot) of the resultant scatter diagram shows the dependence between the two variables.
The method of least squares is used to lay a best-fit line f through the scatter plot.
The pattern (scatter plot) of the resultant scatter diagram shows the dependence between the two variables.